Skip to main content
Visitor II
November 10, 2013
Question

USB hardware with STM8 - library

  • November 10, 2013
  • 4 replies
  • 3534 views
Posted on November 10, 2013 at 19:22

Hello,

Is there any software library that allows to build USB hardware with STM8 microcontroller without any additional chip?

I am looking it but I have not found anything so far. Such library would greatly improve value of STM8 microcontrollers (and volume of sale) as it would open possibility to construct the broad set of applications.

For Atmel AVR 8bit there are at least two nice solutions that runs on any AVR microcontroller with at least 2 kB of Flash memory, 128 bytes - e.g. ATTiny2313.

1 - V-USB is a software-only implementation of a low-speed USB device for Atmel�s AVR microcontrollers

2 - LUFA (Lightweight USB Framework for AVRs, formerly known as MyUSB)

If you have such library you can build a lot of useful applications e.g.

Android Accessory Host

Audio In Device

Audio In Host

Audio Out Device

Audio Out Host

Dual Virtual Serial Device

Generic HID Device

Generic HID Host

Joystick Device

Joystick Host

Keyboard Device

Keyboard/Mouse Device

Keyboard Host

Keyboard Host/Device Dual Mode

Mass Storage Device

Mass Storage/Keyboard Device

Mass Storage Host

MIDI Device

MIDI Host

Mouse Device

Mouse Host

Printer Host

RNDIS (CDC) Ethernet Device

RNDIS (CDC) Ethernet Host

Still Image Host

Virtual Serial Device

Virtual Serial Host

Virtual Serial/Mass Storage Device

Virtual Serial/Mouse Device

Why is no similar solution for STM8? Is STM8 family of microcontrollers somewhat worse than AVR family?

Regards and thanks,

Jane

#stm8-usb #stm8 #usb #library
    This topic has been closed for replies.

    4 replies

    Visitor II
    November 23, 2013
    Posted on November 23, 2013 at 21:31

    Hi again,

    I am thinking over implementing USB device firmware for STM8.

    Do you see any missing functionality in STM8 family that does not allow to create USB device firmware for STM8?

    If AVR can have USB firmware, why STM8s cannot have?

    Regards,

    Jane

    Visitor II
    November 24, 2013
    Posted on November 24, 2013 at 08:35

    Hello Jane.

    I think that STM8 hardware is as good as AVR one.

    Therefore, a USB library for STM8 is feasible, but it may take a long time to develop and test if you are not well acquainted with STM8 assembler.

    If you need assistance on STM8 assembler and if there are no time limits on development, I'll help you.

    EtaPhi

    Visitor II
    March 1, 2014
    Posted on March 01, 2014 at 07:56

    I wrote a program receiving and transmitting data to the microcontroller STM8

    (Tested on STM8S103F3)

    But so far not implemented in full support of the protocol itself USB :(

    Source code and

    description in

    Russian

    (very

    short).

    http://ziblog.ru/2014/02/22/programmnyiy-usb-na-stm8-chast-2.html

    Visitor II
    March 2, 2014
    Posted on March 02, 2014 at 18:19

    Hi,

    Good job! Thank you. The code looks nice.

    I advice you to publish the code on one of the most popular code repository  https://github.com/  or http://sourceforge.net/

    If you document code well in English and publish code on repository it will allow you to build community of volunteers that will help you to improve project. And it such case nobody will ever forget that you created the first implementation of USB protocol on  STM8 microcontrollers. Maybe you will be able to gather some support from ST company. Who knows?

    Some schematics like these on AVR V-USB webpage would be also helpful for some people.

    Thank you again. Keep up this valuable job.

    Best regards,

    Jane