Using SWIM from STM8S Discoveryboard for STM8AF
Hello community,
after unsoldering the solderbridges of the STM8S-Disco-Board, I try to connect the SWIM to a STM8AF Chip. I read in the manueal, that this is not possible (only for STM8S-Family). But after trying it, I could flas Code on the µC and Debug it with the STVD. For example, a counter in my programm ist counting up :)
But if I want to switch Timer1-Output-Pin from LOW to HIGH, nothing happens.
Is ist possible,, that I can program the µC and it is running without errors, but the mapping of the GPIOs are not correctly done?
Is there a influence of the SWIM-adapter even if I had chosen the STM8AF-Chip in STVD?
Thank you all, Steffen