Which libraries should I add to the project?
Hello.
I'm trying to get started with stm8s series with IAR compiler that I'm not very good at.
So for the first project just trying to on and off a single LED to see if everything is ok or not.
I used Keil before this in ARM MCUs, that at first I the compiler asked me if I want to add the startup file or not.
So every time I pushed the yes button and everything was ok.
But IAR does not do this.
So I wanted to know what libraries should I add to the project?
I have to mention that I'm just using the registers and not any standard libraries.
The MCU I'm working with is an STM8S105k4t6.