Why doesn't the COSMIC compiler start?
I downloaded and installed the COSMIC stm8 free compiler (http://cosmicsoftware.com/download_stm8_free.php).
I requested and received a license.
I copied the license file to the appropriate folder.
However, the compiler does not start.
It does not start from ST Visual Develop.
I tried to run it on the command line, from the folder in which it is located (D:\Program Files\COSMIC\FSE_Compilers\CXSTM8).
I see error: "D:\Program Files\COSMIC\FSE_Compilers\CXSTM8\cxstm8.exe not a valid Win32 application"
I use Windows XP SP3.
I tried 3 times reinstall compiler. And i got same error.