Skip to main content
Visitor II
June 24, 2020
Question

Why is the option tab in the ICD MCU configuration window not showing?

  • June 24, 2020
  • 0 replies
  • 568 views

I am using STVD on a Win10 and when I want to debug a program on a MCU. When the read out protection is set the pop up window named "ICU MCD configuration" showes up. There used to be two tabs where one was showing the option bytes where you could reset the read out protection. The window is even shown in the documentation under "6.1.4 Configuring option byte settings". As of now the tab is missing and i have to use the seperate programmer every time to reset the ROP.0693W000001rO6mQAE.jpgWindow as seen in the documentation.0693W000001rO6cQAE.jpgWindow as seen when I start debuging.

    This topic has been closed for replies.