Will the STM8S005K6T6CTR be a good fit for my requirements?
I would like to use the STM8S005K6T6CTR in my next project. This is my first project outside of the arduino ecosystem, so sorry for bad questions(if any) .
The MCU will be responsible for taking care of the following tasks:
1) Driving a 4 digit 7 segment display
2) 4 button water tolerant capacitative touch input
3) Drive a buzzer
4) Drive a relay
5) Drive 6 LEDs
6) A timer with 1.5% accuracy(possible without external resonator?)
Thanks and Regards