OPAMP output: VDDA overconsumption
The STM32L471 Errata document states that: An overconsumption can appear on VDDA in the following conditions:
• a voltage VPAD is applied on PA3 or PB0 with VDDA+ 50 mV < VPAD < VDDA + 600 mV
...
Our application uses PB0 as a GPIO output with a voltage in the range described above. Is that matching the condition 'a voltage VPAD is applied'?