Problem with noise with addressable LEDs Hi! I'm using Inolux_IN-PI554FCH LEDs with a custom PCB, controlled by an STM32H563VGT6.When using the LEDs and setting a colour like 255,0,0 (RGB) the noise generated on the data track is negligible. However, when I set a colour that is not 255, the noise on the data track becomes very high, interfering with the operation of other components. The noise measurements have been taken at the points marked in the following image. Noise measure of colour 255,0,0 (RGB):Measure at mark 1: Measure at mark 2: Noise measure of colour 255,45,13 (RGB):Measure at mark 1: Measure at mark 2: As I mentioned, when producing a colour like 255,0,0 (RGB) or any variant such as 0,255,0 (RGB), the noise on the track is negligible. However, when producing a color that is not 255, such as the case of 255,45,13 (RGB), the noise on the track is too significant to ignore.Currently, with this noise, I am experiencing issues with a capac