Skip to main content
Roadrunner1805
Associate III
January 29, 2024
Question

Readout Protection

  • January 29, 2024
  • 0 replies
  • 614 views

I'm using the BlueNRG-LP and want to enable "Readout Protection". From the reference manual RM0479 it can be enabled by writing the UserKey 0xAAAAAAAA to DATA0/1. In the RF-Flasher 4.3.5 Openocd readout_protection.cfg file writes the UserKey 0xFCBCECCC to DATA0/1. And in the Application note AN5471 it can be enabled via a Bootloader command. So my question is now which one is the correct?