STM32-DISCOVERY Atollic toolset ST-Link debugger not working Posted on November 08, 2010 at 20:51I have the STM32-Discovery board - it appears to be working, lights blinking, etc. When plugged into a USB port on my Windows XP machine, I can see 3 files that direct my browser to the STM website, i.e. USB communications are working.I have downloaded the Atollic lite toolset. I can build the embedded example. It seems to be working except that it appears that the ST-Link debugger is not working.I have successfully updated the ST-Link debugger to the latest firmware version from the STM website. The process reports successful update i.e. communications via USB is ok.The problem seems to be that when the Atollic TrueSTUDIO gdbserver is launched it reports that there is an ''error initializing the ST-Link device'' and exits.Atollic has not replied to questions - can anyone help? Thanks!