10 msps dac and adc stm32 recommendation
Dear Stm32 users,
I currently plan to design an analog function generator and capture System.
The old System used an analog lock in amplifier circuit to excite and capture noisy signals from a measurement source.
For cost and pcb size saving i am considering to switch to a software Version as i can speed up the measurement by using a multisine instead of a swept sine. The frequency range is 10kHz to 1Mhz. A good Resolution is around 1k to 2k Points per decade.
My current plan would be using a function generator with variable frequency to trigger the internal dac and adc at up to 10 MHz. Both using ring buffers. The captured data is stored in an external psram chip for later Analysis. The storage qspi transfer is triggered at half point of euch conversion.
Do you think this is feasable? What do you think would be a viable ic? STM32L4?
P.s.A Sampling rate of a maximum of 10MSPS should suffice.
According to [AN4566](https://www.st.com/content/ccc/resource/technical/document/application_note/6f/35/61/e9/8a/28/48/8c/DM00129215.pdf/files/DM00129215.pdf/jcr:content/translations/en.DM00129215.pdfcs-1.pdf) the maximum Performance of the DAC of L4 is 10MSPS and of L4+ 12MSPS.
The L4 has a maximum ADC Frequency of 5.3 MSPS. I thought about using dual alternating trigger mode. If necessary, I can feed the signal to multiple channels and pins.
My current biggest concern are the DMA channels, as both ADC and the DAC need DMA channels as well as any additional memory chip.
Best regards,
Seren