8 pulse pin outputs on the STM32F407 (Drive GPIO with basic timer?)
Hi, I have an application where I need to send send signals to 8 stepper drivers on my STM32F407 Discovery board. Each stepper driver requires an independent PULSE, DIRECTION, and SLEEP signal. DIRECTION and SLEEP are trivial GPIOs high/low. I have used timers in the past to drive the PULSE pins for these stepper drivers with success.
I am wondering if I can control all 8 independent PULSE pins with a single board. There are 8 timers on the STM32F4 . TIM2, TIM5 TIM9 and TIM14 are General-purpose timers and TIM1 and TIM8 are Advanced-control timers. I am confident I can drive 6 independent PULSE signals with these 6 timers. TIM6 and TIM7 are basic timers without input/output functionality.
Is there is a way to drive two other pins with the basic timers 6 and 7 or is there another way to get up to 8 independent PULSE signals?