A bit disappointed about the STM32H7R/S lines
Dear ST,
I was pleased to hear about the new STM32H7R/S lines, especially with the new graphic acceleration features in the R-line.
However, and perhaps I have missed something, but I have to admit I am also disappointed about the absence of large sized internal RAM and FLASH. I was hoping to see a new boosted H7-version with large capabilities of internal memory similar to some devices in the STM32U5-series. A minimum of 4 MB RAM + 4 MB FLASH would probably have made the need for external memory interfacing unnecessary in 9 out 10 applications and making the device work perfect with large screen resolutions out-of-the-box.
Instead, the new STM32H7R/S lines would now need to be interfaced with BOTH external RAM and FLASH. Also, it seems to lack support OCTO SPI interface which would lead to a more complex PCB design with parallel memory interfacing.
So, I am curious to hear if there are any plans for making a device version with larger internal RAM and FLASH like the U5-series, preferable also in a LQFP-package with low pin count like 100 or 144 pins?