Skip to main content
Graduate
April 24, 2025
Solved

A/D input signal saturated at 3.3V, despite "5 V tolerant I/O"

  • April 24, 2025
  • 3 replies
  • 886 views

Dear all,

 

Dear all,

I use a NUCLEO_H7A3ZI_Q, connected through an external Arduino/Zio-type connector to an external signal generator, which outputs a constant voltage level.

  • the input channel of the μCU appears to be saturated to 3.3V; it shows this value, even if I increase the incoming voltage to e.g. 4.0V.
  • However, the manual DS13313 states, that this channel should be 5.0V tolerant (see attachment)

Could this be related to the caution notice from the UM2408 Manual (see attachment)

 

I wonder how the adapter board is able to saturate the value, if that is true...

 

Many thanks

L.A.

    This topic has been closed for replies.
    Best answer by Ozone

    Here a snipped from a datasheet of another STM32 - I don't have nor use a H7 :

    Ozone_0-1745493460998.png

    Check the respective section in the datasheet of your MCU variant.

    And check for footnotes like this :

    Ozone_1-1745493702228.png

    The term "5V-tolerant" does not mean "operating properly with 5V applied".
    And analog pins are explicitely exempt anyway.

    3 replies

    Explorer
    April 24, 2025

    Of course.

    Read the datasheet.

    LysAnAuthor
    Graduate
    April 24, 2025

    So I disconnected the adapter, and even now my readings don't climb above 3.3V, when I apply a higher voltage directly at pin PA3 (ADC_123_INP10) of my Nucleo board. Anyone has an explanation for that?
    Cheers

    OzoneAnswer
    Explorer
    April 24, 2025

    Here a snipped from a datasheet of another STM32 - I don't have nor use a H7 :

    Ozone_0-1745493460998.png

    Check the respective section in the datasheet of your MCU variant.

    And check for footnotes like this :

    Ozone_1-1745493702228.png

    The term "5V-tolerant" does not mean "operating properly with 5V applied".
    And analog pins are explicitely exempt anyway.

    Explorer II
    April 24, 2025

    Datasheet says V_AIN <= V_Ref+ <= V_DDA <=3.6V.