Skip to main content
Explorer
February 2, 2024
Solved

About Parallel Communication

  • February 2, 2024
  • 3 replies
  • 1932 views

We want to do parallel communication. How can we do parallel communication with the following microcontroller?
Is it possible to perform parallel communication by using I2C function?

[IDE]STM32CubeIDE 1.14.0
[MCU] STM32F412VGT6

    This topic has been closed for replies.
    Best answer by AScha.3

    Basically yes , at low speed some "parallel communication" could be done with just using GPIOs .

    But nothing really useful, or for hi-speed PCI and SCSI bus .

    Just look at the general description of a cpu (or soc) , especially whats written under "communication interfaces " , then you can see, what is there : (on H563 , as example here)

     

    AScha3_0-1706867023869.png

    So here the " One 16-bit parallel slave synchronous- interface " could be useful for your idea.

    3 replies

    Technical Moderator
    February 2, 2024

    What do you mean by parallel communication?

    How should a serial bus such as I2C communicate in parallel?

    Regards
    /Peter

    Explorer
    February 2, 2024

    We call communication standards such as PCI and SCSI parallel communication. Is it possible to connect to them with the target mcu?
    Would GPIO be able to achieve this?

     

    [MCU] STM32F412VGT6

    AScha.3Answer
    Super User
    February 2, 2024

    Basically yes , at low speed some "parallel communication" could be done with just using GPIOs .

    But nothing really useful, or for hi-speed PCI and SCSI bus .

    Just look at the general description of a cpu (or soc) , especially whats written under "communication interfaces " , then you can see, what is there : (on H563 , as example here)

     

    AScha3_0-1706867023869.png

    So here the " One 16-bit parallel slave synchronous- interface " could be useful for your idea.

    Super User
    February 2, 2024

    Just explain : what is "parallel communication" in your world, but if you obviously want to use a serial port (I2C) ?

    Technical Moderator
    February 2, 2024

    There are many different implementations of PCI and SCSI. As a rule, however, we are talking about current high-speed variants that you cannot handle with bit banging via the GPIOs. It may be possible to discuss your task in more detail if you provide more precise information about what exactly you want to do.