About the DS11532
Hello ST Community team,
On the DS11532:
- The title of the Figure 20 should be changed to avoid any confusion between figure 20 and figure 21.
- Also, the note under figure1 is not really clear since the STM32F767 TFBGA216 for example is not compatible pin to pin with the STM32F469 TFBGA216. So, I think the note should be clearer. It can even point to the application note AN4660 for details.
Could you please have a look.
Best Regards.
II