About the ?LL_AHB1_GRP1_EnableClock ? function of the LL library
Regarding LL_AHB1_GRP1_EnableClock, after setting bit in the function, it is read to "tmprg" and cast to void type. What is the reason for reading?
__STATIC_INLINE void LL_AHB1_GRP1_EnableClock(uint32_t Periphs)
{
__IO uint32_t tmpreg;
SET_BIT(RCC->AHBENR, Periphs);
/* Delay after an RCC peripheral clock enabling */
tmpreg = READ_BIT(RCC->AHBENR, Periphs);
(void)tmpreg;
}