Skip to main content
Explorer
November 20, 2024
Solved

About the negative ref voltage supply to STM32H753ZI

  • November 20, 2024
  • 4 replies
  • 1619 views

Hi,

    The datasheets says (P173) - the VREF s available only on UFBGA176+25 and
TFBGA240+25. When VREF- is not available, it is internally connected to VDDA and VSSA.

 Our ADC input signal goes to both positive and negative. 

Questions:

1. What the part number we should use, which allows VREF? (Negative ref)

2. Is VREF a fixed value or changeable? How is it defined relative to the input signal range?

3. Does NUCLEO-H753ZI board allow our negative ADC input signal in? If so, who is the the range (max + and max -) defined? 

Thank you very much for your help,

 

    This topic has been closed for replies.
    Best answer by jiangfan

    refer to chapter 6.3.20 of datasheet

    DS_STM32H743xI_Rev10_ADC-Vref.png

    4 replies

    ST Employee
    November 21, 2024

    Refer to chapter 9 Ordering information, for part number with VREF-

    Explorer
    November 21, 2024

    Thanks

    "Refer to chapter 9" - In which document? 

    Thanks again

    ST Employee
    November 21, 2024

    datasheet

    ST Employee
    November 21, 2024

    VREF+ max is Vdda (Max 3.6V), so, I suppose VREF- min is -3.6V

    Explorer
    November 21, 2024

    Thanks,

    VREF+ max is Vdda (Max 3.6V), so, I suppose VREF- min is -3.6V

    What is VREF+ min ?

    What is VREF- max?

    Also -

    Can the input signals on their selected channels of all SAR ADC be sampled synchronously under the same sampling rate?

    Thanks again

     

     

    jiangfanAnswer
    ST Employee
    November 21, 2024

    refer to chapter 6.3.20 of datasheet

    DS_STM32H743xI_Rev10_ADC-Vref.png

    ST Employee
    November 21, 2024

    if understand correctly, NUCLEO-H753ZI board does not support negative ADC input if ADC input directly connected to STM32H753ZI pin. User may use OPAMP to shift negative input ~ positive input => 0 ~ Vdda, for example -5V ~ +5V => 0V ~ 3.3V.

    Explorer
    November 21, 2024

       The datasheets (STM32H753ZI) says (P173) - the VREF s available only on UFBGA176+25 and
    TFBGA240+25

        Should we specify it when order (STM32H753ZI)?  

        Thanks

    Super User
    November 21, 2024

    The package type & number of pins is part of the ordering code:

    AndrewNeil_0-1732190973113.png

    https://www.st.com/resource/en/datasheet/stm32h753zi.pdf#page=348

    Explorer
    November 21, 2024

    Thank a lot!!