Accessing Radxa eMMC Module (eMMC 5.1) on STM32H750B
Hello,
I am seeking guidance on how to interface and access a Radxa eMMC Module, which operates on the eMMC 5.1 specification, with either the STM32H750B-DK development kit or the WeAct Studio STM32H750VBT6 development board. I also have a Radxa eMMC to uSD converter, which allows the eMMC module to interface via a microSD card slot. Any suggestions or step-by-step guidance would be greatly appreciated, as I aim to integrate this storage solution into my project.

- Since the WeAct board has a microSD card slot, can I directly insert the Radxa eMMC module (via the eMMC to uSD converter) into this slot and access it using the STM32’s SDMMC peripheral?
- Are there specific configurations or drivers required in STM32CubeIDE to initialize and communicate with the eMMC module through the microSD interface?
- Are there any known compatibility issues with the eMMC 5.1 protocol when interfaced via the uSD converter on this board?
- How should I configure the SDMMC peripheral (e.g., 1-bit, 4-bit, or 8-bit mode) to ensure compatibility with the eMMC module through the uSD converter?