ADC Conversion time of STM32U5A5
Hello,
i've implemented a routine to measure some ADC channels with the MCU STM32U5A5ZJ.
After one measurement is finished (interrupt triggers after conversion) i start the conversion for the next channel.
Settings:
ADC conversion: Single conversion mode, conversion length: 1 (i just want one conversion per channel)
ADC CLK: 1843200Hz
Sample Time: 5 Cycles
14 bit mode: 17 Cycles
TCONV = (5 + 17) ADC clock cycles = 22 ADC clock cycles = 11,9us
To check the whole conversion time i toggled a pin at the start and end of conversion and looked at the signal on the oscilloscope.
My result is 50us for the conversion time.
My question is:
Why is the conversion time so long? I expected 11,9us and i got 50us!
I appreciate any help.
LG
Shaheen