ADC conversion using End of Conversion Selection?
Good evening....
I would like to do an A/D conversion on Channel 9 and Channel 10. I have a timer that goes off every second and within this ISR I call HAL_ADC_Start_IT. The ISR gets called upon conversion complete. Now the question is End of Conversion Selection: Should it be 'End of Single Conversion' or 'End of Sequence of Conversion'?? Even though I am sampling multiple channels is this considered a sequence or a single conversion of multiple channels, given that I am using a timer to trigger this single event every second???? This is not explained well and confusing.
Thanks
Steve