Skip to main content
Visitor II
February 24, 2025
Question

ADC doesn't work

  • February 24, 2025
  • 3 replies
  • 536 views

Hi all, 

I have created a new project for the STM32U575RIT6 microcontroller using the attached .ioc file. On top of the auto-generated code, I have made the following modifications:

In main.c:

 

 

 

 while (1)
 {
	uint32_t bits = 0;
	uint16_t adc_value = 0;
	uint16_t n_samples = 50;
	do
	{
		// Start the conversion process
		HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
		HAL_ADC_Start(&hadc1);
		HAL_Delay(10);

		// Average value of nSamples
		if (HAL_ADC_PollForConversion(&hadc1, 5000) == HAL_OK)
		{
			adc_value = (uint16_t) HAL_ADC_GetValue(&hadc1);
			if (adc_value > 0)
			{
				bits += adc_value;
			}
		}
		}
	}while(bits == 0);
	HAL_Delay(1000);
}

 

 

In stm32u5xx_hal_msp.c:

 

 

void HAL_MspInit(void)
{

 /* USER CODE BEGIN MspInit 0 */

 /* USER CODE END MspInit 0 */

 __HAL_RCC_PWR_CLK_ENABLE();

 /* System interrupt init*/

 /* USER CODE BEGIN MspInit 1 */

 HAL_PWREx_EnableVddA();
 HAL_PWREx_EnableVddIO2();
 /* USER CODE END MspInit 1 */
}

 

 


However, the ADC always reads 0. I have verified the following:

  • ADC Configuration: The ADC is set up correctly, with the appropriate channel and reference voltage selected.
  • Pin Setup: The pin connected to the ADC channel is initialized as an analog input.
  • Input Signal: A valid analog signal is present at the ADC input pin (1.6V).

Has anyone experienced similar issues or have suggestions on how to resolve this? Any help or advice would be greatly appreciated.

Thank you in advance for your assistance.

    This topic has been closed for replies.

    3 replies

    Super User
    February 24, 2025

    > Has anyone experienced similar issues or have suggestions on how to resolve this? 

    You haven't actually described what your issue is. Only that it "doesn't work".

    Calibration should only be called once.

    proyoAuthor
    Visitor II
    February 25, 2025

    Hello, thanks for your suggestion. As I mentioned in my original post, the issue is that the ADC value (adc_value) is always 0, even though there is a valid 1.6V analog signal at the input. I've tried calling the calibration function just once, but the result remains unchanged.

    I don't really know why this is happening, so unfortunately I can't provide any more information. Any further ideas or suggestions on how to troubleshoot this behavior would be greatly appreciated. Thanks in advance for your help!

    Super User
    February 25, 2025

    Code seems correct otherwise. If HAL_ADC_PollForConversion returns HAL_OK, the ADC is converting a voltage from somewhere.

    Could be that the board is damaged, could be that your assumptions are incorrect. Set the pin as output and toggle and measure with a multimeter to verify connectivity.