ADC issue : Resister value returns the address.
Hi. I'm using Keil5.
ADC encountered an error in my program(from function HAL_ADC_PollForConversion), so I tried debugging and found the following problems.

As shown above, the register value in CFGR1 returns the address.
In a typical program(Operating Normally), the register value should be returned properly as shown below.

Why is this problem occurring? I looked into the manual and found nothing about these problems.
I haven't modified the contents of the Driver, and the settings for both programs are the same.