ADC peripheral clock configuration
I am using STM32F429VIT6. Configured SystemCoreClock 168MHz and APB2 clock is 84MHz. I accidentally configured ADC peripheral with "ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;" but datasheet says max ADC frequency is 36MHz. I am wondering about my ADC peripheral clock:
- Is it running at 42MHz with overclocking? or
- Is it running with max freq. so it is 36MHz? or
- Is it running with typical freq. so it is 30MHz? or
- Is it ignore ADC_Prescaler_Div2 and process it with ADC_Prescaler_Div4 so it is 21MHz?