Skip to main content
Graduate
November 26, 2023
Solved

ADC_Sequencer not fully configurable: STM32G0

  • November 26, 2023
  • 2 replies
  • 3587 views

Can any of the expert share an example of ADC configured in Sequencer not fully configurable mode please?Its hard to find the solution .As the project had predefined prototype I need to sort it out with the configuaration and mandatory to use PA12 (adc_in_15)and PA11(adc_in15).Please

    This topic has been closed for replies.
    Best answer by TDK

    You're missing this line in your initializations:

     sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;

    Take a look at the ADC_CHSELR register after configuring to ensure it only has a single bit set corresponding to the channel you want.

    You must calibrate the ADC before using it, if you care about the results being accurate.

    2 replies

    Super User
    November 27, 2023

    Does the code that CubeMX generates here not work for this case? What in particular are you having trouble with?

    It's generally a lot easier (for contributors) to post your code and debug that than for someone to create an entire example that might solve your problem.

    > PA12 (adc_in_15)and PA11(adc_in15)

    Is this a typo? Surely both pins aren't channel 15 input.

    SRAM.11Author
    Graduate
    November 27, 2023

    hi,Yes its a typo sorry about that ch15 and ch 16

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2023 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    ADC_HandleTypeDef hadc1;
    
    /* USER CODE BEGIN PV */
    uint16_t Tsense_raw=0,Batmon_raw=0,Vbat_raw=0;
    float Tsense=0,Batmon=0,Vbat=0;
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_ADC1_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    void Get_Tsense(void)
    {
    	ADC_ChannelConfTypeDef sConfig = {0};
    	 sConfig.Channel = ADC_CHANNEL_0;
    	 sConfig.Rank = 1;
    	 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
    	 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
    	 {
    	 Error_Handler();
    	 }
    	 HAL_ADC_Start(&hadc1);
    	 		HAL_ADC_PollForConversion(&hadc1, 1000);
    	 		Tsense_raw=HAL_ADC_GetValue(&hadc1);
    	 		Tsense=(Tsense_raw*3.3)/4095;
    	 		HAL_ADC_Stop(&hadc1);
    	 				HAL_Delay(100);
    
    }
    void Get_Vbat(void)
    {
    	ADC_ChannelConfTypeDef sConfig = {0};
    		sConfig.Channel = ADC_CHANNEL_16;
    
    		 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
    		 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
    		 {
    		 Error_Handler();
    		 }
    		 HAL_ADC_Start(&hadc1);
    		 HAL_ADC_PollForConversion(&hadc1, 1000);
    
    		 Vbat_raw=HAL_ADC_GetValue(&hadc1);
    		 Vbat=(Vbat_raw*3.3)/4095;
    		 HAL_ADC_Stop(&hadc1);
    		 HAL_Delay(100);
    
    }
    void Get_Batmon(void)
    {
    	ADC_ChannelConfTypeDef sConfig = {0};
    	sConfig.Channel = ADC_CHANNEL_15;
    	 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
    	 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
    	 {
    	 Error_Handler();
    	 }
    	 HAL_ADC_Start(&hadc1);
    	 HAL_ADC_PollForConversion(&hadc1, 1000);
    
    	 Batmon_raw=HAL_ADC_GetValue(&hadc1);
    	 Batmon=(Batmon_raw*3.3)/4095;
    	 HAL_ADC_Stop(&hadc1);
    	 HAL_Delay(100);
    }
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_ADC1_Init();
     /* USER CODE BEGIN 2 */
    
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
    	 Get_Tsense();
    	 Get_Vbat();
    	 Get_Batmon();
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief ADC1 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_ADC1_Init(void)
    {
    
     /* USER CODE BEGIN ADC1_Init 0 */
    
     /* USER CODE END ADC1_Init 0 */
    
     ADC_ChannelConfTypeDef sConfig = {0};
    
     /* USER CODE BEGIN ADC1_Init 1 */
    
     /* USER CODE END ADC1_Init 1 */
    
     /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
     */
     hadc1.Instance = ADC1;
     hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2;
     hadc1.Init.Resolution = ADC_RESOLUTION_12B;
     hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
     hadc1.Init.ScanConvMode = ADC_SCAN_SEQ_FIXED;
     hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
     hadc1.Init.LowPowerAutoWait = DISABLE;
     hadc1.Init.LowPowerAutoPowerOff = DISABLE;
     hadc1.Init.ContinuousConvMode = ENABLE;
     hadc1.Init.NbrOfConversion = 1;
     hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
     hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
     hadc1.Init.DMAContinuousRequests = DISABLE;
     hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
     hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
     hadc1.Init.OversamplingMode = DISABLE;
     hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
     if (HAL_ADC_Init(&hadc1) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Configure Regular Channel
    
     sConfig.Channel = ADC_CHANNEL_0;
     sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
     if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Configure Regular Channel
    
     sConfig.Channel = ADC_CHANNEL_15;
     if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Configure Regular Channel
    
     sConfig.Channel = ADC_CHANNEL_16;
     if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN ADC1_Init 2 */
    
     /* USER CODE END ADC1_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOA_CLK_ENABLE();
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */

    .I have tried with all possible ways also by dma method for all  i am getting same values read by all channels.

    TDKAnswer
    Super User
    November 27, 2023

    You're missing this line in your initializations:

     sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;

    Take a look at the ADC_CHSELR register after configuring to ensure it only has a single bit set corresponding to the channel you want.

    You must calibrate the ADC before using it, if you care about the results being accurate.

    SRAM.11Author
    Graduate
    November 27, 2023

    sorry to be a pain but still having issues. I couldn't able to read multiple channel in Sequencer not fully configurable mode.so I asked for an example