Skip to main content
Explorer
November 24, 2023
Solved

AN5290 Possible Typo in LDO configuration for VDD > 2.5 V Section

  • November 24, 2023
  • 2 replies
  • 1215 views

AN5290 discusses a workaround for the "When VDD exceeds 2.5V in LDO configuration a glitch on HSE may create a hard fault on M4/M0" issue identified in the errata. In the AN5290 section titled "1.2 LDO configuration for VDD > 2.5 V"  recommends:

The recommended values (see Figure 3) are:
• Inductance: 1.8 ± 0.1 nH, 6 GHz ± 15% self-resonance frequency, 1000 mA rated
current (for example, Murata LQG15HS1N8B02)
• Resistor: 2.2 Ω, able to support 1 W for 5 ns (for example, Vishay D10/CRCW0402e3)

However in Figure 3 it shows a 1.2nH inductor.

Not sure if this is the correct form to identify these discrepancies, so if someone could let me know the best location for these issues that would be great. 

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hi again @alexRossRBR 

    Thank you for having reported this issue.

    An internal ticket (number: 167173) is submitted to escalate this issue internally for check and analysis.
    (PS: number 167173 is an internal tracking number and not available outside of ST).

    Best Regards.

    STTwo-32

    2 replies

    Technical Moderator
    November 24, 2023

    Hello @alexRossRBR 

    thank you for your request.  I will check this internally and come back to you as soon as possible.

    Best Regards.

    STTwo-32

    STTwo-32Answer
    Technical Moderator
    November 24, 2023

    Hi again @alexRossRBR 

    Thank you for having reported this issue.

    An internal ticket (number: 167173) is submitted to escalate this issue internally for check and analysis.
    (PS: number 167173 is an internal tracking number and not available outside of ST).

    Best Regards.

    STTwo-32