Skip to main content
Super User
March 19, 2024
Solved

AN6091 ('L0->'U0 migration) comments

  • March 19, 2024
  • 8 replies
  • 2611 views

This is not a discussion on the 'U0 as such (that'd need some time to sink in); just comment on the 'L0->'U0 migration document, AN6091. It's a very detailed and extensive document, and following items are just relatively insignificant minor issues/typos:

- after an optimistic introduction in Pin compatibility chapter (The STM32U0 and STM32L0 series share a high level of pin compatibility.) the subsequent subchapters basically say "nah, forget about it". The TSSOP-20 package is entirely different. On the QFN packages, 'U0 does not have VSS on the exposed pad, so two pins are simply used as VSS, making drop-in impossible. These make the optimistic intro somewhat less substantiated.

- pity that the consumption - which is supposed to be the main selling point of 'U0 - is not presented side-by-side with 'L0, making it hard to compare

- Tab.16 description of reset state of GPIOs is incorrect as 'L0 has Analog as defaults too;  instead of 'L0 mentions 'L1 , clearly a fossil (see also below for chapter 6.8)

- Tab.16 when talks about timers, fails to highlight a - IMO very important fact, that contrary to 'L0 which has no 32-bit timers, TIM2 in 'U0 is 32-bit

- Tab.23 incorrectly split "battery backup domain" in the first column

- Tab.24 RTC_TAFCR (L1) -> RTC_TAMPCR etc. is a fossil

- Chapter 6.8 talks about Routing Interface. There's no RI in 'L0, this is some fossil from 'L1

- Chapter 6.11 should've mentioned the different erased state of FLASH (0x00 'L0 vs. 0xFF 'U0), as this is a quite surprising/unexpected thing, and this might be potntial issue when migrating

- Chapter 6.14 says, "Two serial audio interfaces (SAI) replace the I2S interface of the SPI on STM32U0 devices.", yet table 31 for 'U0 says "NA", and there seem to be no SAI mentioned in the 'U0 DS either.

- Tab.35 for 'U0 states 200 mA/Msps consumption; that's certainly too much, should probably be 200uA/Msps

- Tab.37 for 'L0 says "COMP1 fixed threshold", I don't understand what "fixed threshold" is supposed to mean there

- Tab.38 Opamp - there's no opamp in 'L0, yet the "features" row contains them in 'L0, obviously moved inadvertently from the 'U0 column, and there's a funny line in "configuration row" saying that registers are not organized in the same way as in 'L0...

JW

PS. @Lina_DABASINSKAITE , we will need a STM32U0 Series tag ("label") here.

    This topic has been closed for replies.
    Best answer by STOne-32

    Hi @waclawek.jan ,

    Waw ! thank you very much for the quick feedback - less than  4 hours after announcing our Newest STM32U0 ULP and entry cost series after the STM32L0.  Much appreciated and will be followed internally using this tracking number 176522  

    Ciao

    STOne-32 

    8 replies

    STOne-32Answer
    Technical Moderator
    March 19, 2024

    Hi @waclawek.jan ,

    Waw ! thank you very much for the quick feedback - less than  4 hours after announcing our Newest STM32U0 ULP and entry cost series after the STM32L0.  Much appreciated and will be followed internally using this tracking number 176522  

    Ciao

    STOne-32 

    Community Manager
    March 19, 2024

    Hi @waclawek.jan , 

    the label has been included! 

    Thanks,
    Lina

    Super User
    March 19, 2024
    Graduate II
    March 19, 2024

    Table 27 also talks of "– Each page: 8 rows of 256 Kbytes."

    ST Employee
    March 22, 2024

    Thank you for this feedback, the update of document is already in process since that and new revision will be released soon.

    ST Employee
    March 26, 2024

    Hi Wek, please note that revision two has been published Friday evening, embedding comparison of the consumption and also multiple images about the pinout similarities and differences.

    Thanks for the valuable feedback and proposals! 

    Link: Migrating from STM32L0 to STM32U0 MCUs - Application note

    Technical Moderator
    March 26, 2024

    Thank you Very much @Viktor POHORELY  and also to @waclawek.jan  & @Uwe Bonnes  to Close the topic and new release of the application note in a record timing of 3 days !

    STOne32_0-1711451071964.png

     

    Super User
    March 26, 2024

    Thanks, @Viktor POHORELY !

    Jan