Any STM32 with Split Power SPI Domains (1.8V & 3.3V IOs) ?
I’m working on a design where I need to communicate with two SPI devices that operate at different logic levels:
1) A sensor running at 1.8v logic (need SPI + 2 other lines, all at 1.8v)
2) Everything else on my board, preferably running at 3.3v, I will need CAN, UART, and another SPI.
I’m trying to avoid level shifters if possible (and avoid sourcing 1.8 V CAN/UART transceivers). Ideally, I’d like to use an STM32 that has split power domains, both with SPI peripherals.
So far, I’ve found that the STM32L496QI supports SPI on both the main VDD rail and the VDDIO2 rail (which can be independently run at 1.8 V), which fits the bill. The only issue is that it’s a 100-pin part, which is way more than I need for this design.
What I’m looking for:
- STM32 with VDDIO2 or similar
- SPI on both 1.8V and 3.3V-capable banks
- Preferably 64 pins or less
Thanks,
Sameer