Skip to main content
Visitor II
July 10, 2024
Solved

Baud rate of 4Mbps

  • July 10, 2024
  • 1 reply
  • 1687 views

Hello everybody,

This is my first post hope i wll get the answer.

I am building a spectrometer for which i am using a stm32f401re board and i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps so do i need to use 4Mbps baud rate to read that and if so how to achieve such higher baud rates.

Thank you.

    This topic has been closed for replies.
    Best answer by AScha.3

    From ds:

    AScha3_0-1720601963254.png

     

     

    So whats the problem?

    1 reply

    Technical Moderator
    July 10, 2024

    Hello and welcome to the community.


    i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps

    Not clear! Is it over a protocol communication? which one?

     

    000harshaAuthor
    Visitor II
    July 10, 2024

    Yes it is over UART

    AScha.3Answer
    Super User
    July 10, 2024

    From ds:

    AScha3_0-1720601963254.png

     

     

    So whats the problem?