BOOT0 on STM32U083
I have a custom board with an STM32U083KCU6 MCU - see schematics below

VBAT = +3.6V
I have 2 boards:
1. board: I flashed it via SWD but forgot to enable it in STM32CubeMX, which means that I'm not able to flash it again via SWD
2. Board: This time, I remembered to enable SWD inside STM32CubeMX and was able to flash it successfully. It worked fine for a long time, but now it suddenly seems like my ST-LINK V2 programmer is no longer able to flash it for some reason...
NRST is connected to RST on the ST-LINK V2 programmer.
I can use the same ST-LINK V2 programmer to flash a STM32U083 Nucleo board, so it does not seem like the ST-LINK V2 programmer is broken
STM32_Programmer_CLI -c port=SWD sn=223215051117303030303032 -d
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------
libusb: warning [libusb_exit] device 4.76 still referenced
libusb: warning [libusb_exit] device 4.75 still referenced
libusb: warning [libusb_exit] device 4.74 still referenced
libusb: warning [libusb_exit] device 4.73 still referenced
libusb: warning [libusb_exit] device 4.72 still referenced
libusb: warning [libusb_exit] device 4.1 still referenced
libusb: warning [libusb_exit] device 3.1 still referenced
libusb: warning [libusb_exit] device 2.2 still referenced
libusb: warning [libusb_exit] device 2.1 still referenced
libusb: warning [libusb_exit] device 1.118 still referenced
libusb: warning [libusb_exit] device 1.5 still referenced
libusb: warning [libusb_exit] device 1.3 still referenced
libusb: warning [libusb_exit] device 1.124 still referenced
libusb: warning [libusb_exit] device 1.127 still referenced
libusb: warning [libusb_exit] device 1.13 still referenced
libusb: warning [libusb_exit] device 1.126 still referenced
libusb: warning [libusb_exit] device 1.125 still referenced
libusb: warning [libusb_exit] device 1.123 still referenced
libusb: warning [libusb_exit] device 1.121 still referenced
libusb: warning [libusb_exit] device 1.122 still referenced
libusb: warning [libusb_exit] device 1.120 still referenced
libusb: warning [libusb_exit] device 1.119 still referenced
libusb: warning [libusb_exit] device 1.117 still referenced
libusb: warning [libusb_exit] device 1.14 still referenced
libusb: warning [libusb_exit] device 1.1 still referenced
ST-LINK SN : 223215051117303030303032
ST-LINK FW : V2J45S7
Board : --
Voltage : 3,16V
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug AuthenticationI have soldered a wire between BOOT0 and VBAT, but am still not able to connect to it via SWD.
Note that the UART is working on board 1, and I am to receive messages from the MCU, which means it has power
Is there anything I'm missing to be able to flash it again via SWD, or what are my options?