Skip to main content
Graduate
January 7, 2025
Solved

BOOTING STM32F469

  • January 7, 2025
  • 6 replies
  • 1476 views

@STOne-32 , @Peter BENSCH@Tesla DeLorean 

HI! I have my wiring below and I wonder what is wrong with it. Hope someone can give me some help!! my BOOT0 -> LOW, PDR_ON -> HIGH, BYPASS_REG -> LOW. And I have the following connections to the ST LINK:

NRST - SWDIO - SWCLK - TRACESWO.

kicad_cropped.jpgkicad_1.jpg

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    Sounds like it's not powered up

    VCAP should be 1.25V at viability

    NRST should be pulled high internally to 3.3V or VDD

    Make sure the PIN 1 is correctly orientated, bottom left corner with readable text on the IC, don't confuse with injection relief ports. Picture of the part on the board would be instructive.

    BYPASS_REG : LOW

    PDR_ON : HIGH

     

    6 replies

    Graduate II
    January 7, 2025

    https://community.st.com/t5/stm32-mcus-products/boot-standalone-stm32f469iit6/td-p/758301

    Please see my question/response at the end

    Check part orientation

    Check voltage present on VCAP pin, and capacitors

    Check voltage observed on NRST pin

    Provide a schematic, constrained to the STM32 if that's simpler, so we can better understand what you've built.

    A large, clear and in-focus picture of the board with the part in-situ will also be illustrative.

    The ST-LINK expects to see a target voltage on pin 1 or 2 of the standard JTAG 20-pin connector.

     

    If you're getting connectivity issues in STM32 Cube Programmer, please show that whole screen, along with error message.

    Graduate
    January 7, 2025

    @Tesla DeLorean 

    I Got this:

    (I Have the same values at the pin and at the capacitor)

    VCAP2 -> 360mV when I insert the probe, then it drops to 312mV.

    VCAP1 -> 480mV.

    NRST -> 396mV.

    The total drawn read in the power supply is 0.07A.

    I took closer pictures, and FYI, NRST goes from the switch (I was unsure what to do with it, so I put a switch to manipulate it.) to the ST-LINK. If any question seems odd, I apologize, this is my first time trying to design a PCB. I am a CS student and therefore I have never worked so close to the hardware beforeGND.jpgPOWER.jpgST-LINK.jpgVCAP.jpgVDA.jpg. Thank you!

     

     

     

    Graduate II
    January 7, 2025

    Sounds like it's not powered up

    VCAP should be 1.25V at viability

    NRST should be pulled high internally to 3.3V or VDD

    Make sure the PIN 1 is correctly orientated, bottom left corner with readable text on the IC, don't confuse with injection relief ports. Picture of the part on the board would be instructive.

    BYPASS_REG : LOW

    PDR_ON : HIGH

     

    Graduate II
    January 7, 2025

    f469_pin1.jpg

    Graduate
    January 7, 2025

    @Tesla DeLorean 

    Also... this is my debugger configuration and the error I get:

    conf.jpgerror.jpg

    Graduate
    January 7, 2025

    @Tesla DeLorean I have a little concern about the pin orientation. I know the dot marks the pin1, but I have 3 dots on the MCU, and therefore I assumed the pin 1 would be on the top left, as the top being oriented in a way that I can read the name of the chip. Did I do it upside down?

    Graduate II
    January 7, 2025

    See image I posted above at same time you posted this.

    Picture of yours would also be instructive as to what you've built..

    Graduate
    January 7, 2025

    Oh OMG, mine is upside down then! :face_with_tears_of_joy::face_with_tears_of_joy:

    I will, solder it in the right place now. I will let you know how it goes, appreciate it!!!!

    Graduate
    January 8, 2025

    @Tesla DeLorean Hey dude! It worked! I got some issues later with the debugger configuration, but I was able to make some lights blink :D. Thank you!