BootLoader and Programming Hardware requirements for custom STM32H753 board
If I have a bare h753 MCU on my custom board. What connection in terms of communication peripherals and connectors do I need to achieve. Basically, I want to bootload the MCU. The next step is to be able to program, monitor, test simultaneously. From my understanding, I need to have a JTAG/SWD pinouts/connector on the PCB to be able to bootload the MCU which can also be used to program/monitor the MCU. Upon reading the AN2606, I can bootload the MCU with SPI or CAN also, am I right in assuming that? Also while working with the nucleo board for the same, whenever I wanted a print statement on the computer I used UART, so do I need an USB-UART bridge to interface between USB data lines and initialized UART pins on the MCU? currently I am interfacing the USB data lines after required ESD protection directly to the USB_OTG_FS peripherals initialized separately.