Bootloader for STM32F746 for firmware and QSPI
Apparently I can not easily update my application firmware for stm32F746 toughGFX app with just one Bin file.
I have written a bootloader for an SD card. It loads firmware at 0x08040000.
I am not sure I understand everything that is going on here, so feel free to correct me.
First issue I noticed was the Binfile created by stm32ide was 2G in size compared to the Hexfile that is 13M! I determined this is because it is padding data from internal flash to external QSPI flash starting at 0x90000000
So now I need to break file into two bin parts and load separately, One into internal flash and the QSPI into external? I think I could also use a hex file, but may have to customize it, and try to load that through my bootloader to do the same thing?
Not sure what I need to do, does anyone have any experience with this?