Skip to main content
Explorer
May 23, 2025
Solved

BOR in STM32U083

  • May 23, 2025
  • 3 replies
  • 420 views

Hello,
I found some discrepancy in BOR configuration for STM32U083CCT6 processor between reference manual [1] and HAL implementation [2]. It concerns BOR_LEV[0:2] bits (bits 10:8) in FLASH_OPTR register. The RM [1] talks of four levels (000: 1.7 V, 001: 2.0 V, 010: 2.2 V, 011: 2.5 V, 100: 2.8 V), in HAL [2] bit 8 is used to enable BOR (OB_BOR_ENABLE in stm32u0xx_hal_flash.h, FLASH_OPTR_BOR_EN in stm32u083xx.h), and the next bits (the remaining two) are used to set the level, importantly, the RISING one (00: 2.1 V, 01: 2.3 V, 10: 2.6 V, 11: 2.9 V), and the next two bits (12:11, which are described in the RM as reserved) are used to set the reaction of the BOR circuit to the falling voltage (00: 2.0 V, 01: 2.2 V, 10: 2.5 V, 11: 2.8 V). So the implementation in HAL is wider (based on 5 bits) and seems more advanced than the one given in the RM. I will add that the erratum [3] is silent on this topic.

So, the question is which BOR settings in the STM32U083 processor are correct?

[1] RM0503, Rev 2 (26-Mar-2024), Reference manual, STM32U0 series advanced Arm®-based 32-bit MCUs
[2] STM32CubeU0 Firmware Package V1.2.0 / 30-October-2024
[3] ES0602, Rev 3 (February 2024), Errata sheet, STM32U073xx and STM32U083xx device errata

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hello @KSzcz.2;

     

    Bits 12:11 are reserved. As I mentioned in my last reply the datasheet, STM32Cube_Fw_U0 (stm32u083xx.h and stm32u0xx_hal_flash.h), and STM32CubeMx will be aligned with this description.

    KDJEM1_0-1748508461276.jpeg

     

    Thank you.

    Kaouthar

     

     

    3 replies

    Technical Moderator
    May 23, 2025

    Hello @KSzcz.2 and welcome to the community;

     

    First of all, thank you for posting.

    You can find the correct BOR settings in the below:

    KDJEM1_0-1748011050866.jpeg

    This issue has already been reported internally to align reference manual, datasheet, STM32Cube_Fw_U0 and STM32CubeMX with this description.

    Internal ticket number: 203504 (This is an internal tracking number and is not accessible or usable by customers)

     

    Thank you.

    Kaouthar

    KSzcz.2Author
    Explorer
    May 23, 2025

    Thank you for your reply.


    But what about bits 12:11? They are still assigned as reserved, but both in HAL and also in DS14463 - Rev 2 (18-Mar-2024) in 3.6.2 Power supply supervisor, can be read that "four (level as used) for falling VDD". A piece of stm32u083xx.h below:

    KSzcz2_1-1748026718829.png

     

     

    KDJEM.1Answer
    Technical Moderator
    May 29, 2025

    Hello @KSzcz.2;

     

    Bits 12:11 are reserved. As I mentioned in my last reply the datasheet, STM32Cube_Fw_U0 (stm32u083xx.h and stm32u0xx_hal_flash.h), and STM32CubeMx will be aligned with this description.

    KDJEM1_0-1748508461276.jpeg

     

    Thank you.

    Kaouthar