Bricked two STM32WBA55 NUCLEO boards by flashing in CubeIDE (repeteable)
Hi there,
here what happened with the second board when I repeated the process.
- Generated IOC project with CubeMX for CubeIDE.
- Does not link correctly in CubeIDE, had to add "-z noexecstack"
C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/thumb/v8-m.main+fp/hard/crtn.o: missing .note.GNU-stack section implies executable stack
C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: NOTE: This behaviour is deprecated and will be removed in a future version of the linker

- Build runs, tried to run, the programmer says I have to upgrade the firmware of the Nucleo STLINK.
- Open in upgrade mode, runs correctly.

Back in CubeIDE:
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: C:\Users\u1ds_cm\AppData\Local\Temp\STM32CubeProgrammer_a25184.log
ST-LINK SN : 003800303133511536303739
ST-LINK FW : V3J16M7B5S1
Board : NUCLEO-WBA55CG
Voltage : 3.29V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x492
Revision ID : Rev B
Device name : STM32WBA52/54/55
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0xB1
Opening and parsing file: ST-LINK_GDB_server_a25184.srec
Memory Programming ...
File : ST-LINK_GDB_server_a25184.srec
Size : 275.84 KB
Address : 0x08000000
Erasing memory corresponding to sector 0:
Erasing internal memory sectors [0 34]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:02.475
Verifying ...
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Back in Programmer,

For the record, I was able to connect before the upgrade + flash.
The upgrade mode seems to work still.

Now both boards show all LEDs on continuously.
When I open the simulated USB drive,

Any help?
Thanks in advance.
CubeMX: 6.14
CubeIDE 1.17
CubeProgrammer: 2.19
CubeCLT: 1.18