Skip to main content
Explorer
July 12, 2024
Question

C16 burned in stm32 L010RB

  • July 12, 2024
  • 2 replies
  • 1648 views

IMG_6646.jpeg

While connecting the battery, the ground was inverted with the VCC and vice versa. As a result, this capacitor burned out. I need to know the function of this part and if I can continue to work normally after what happened.

 

    This topic has been closed for replies.

    2 replies

    Super User
    July 12, 2024

    see circuit:

    AScha3_0-1720807706112.png

    C16 and probably U3 needs repacement. (maybe C17 also.)

    Check if connecting USB : st-link and cpu L010 still working (they should).

    Graduate II
    July 12, 2024

    Bulk capacitance on the input side of the regulator.

    It's destroyed itself, so likely not part of the active circuit at this point. Check if it is open-circuit now with a meter.

    I'd expect the board might continue to function, regulation will be less good.

    Do you have the skill/equipment to replace?

    MinaihabAuthor
    Explorer
    July 12, 2024

    How can i Check if it is open-circuit by the meter ?

    Graduate II
    July 12, 2024

    When did your house burn down?

    Put multi-meter in continuity or resistance mode. You don't want it to beep or show low ohm value.