CAN Auto Bus-Off Recovery Not Happening on STM32G474RE MCU
Hello everyone,
I'm currently working with the STM32G474RE MCU and using a CANopen stack. I'm facing an issue where the Auto Bus-Off recovery isn't happening as expected.
When there's a fault on the CAN bus, it correctly transitions to the warning state, then passive, and finally Bus-Off. However, after the fault is resolved, the bus should recover by moving from Bus-Off to passive, warning, and finally back to error-active, but this recovery is not occurring. The Bus-Off state remains even after the fault is restored.
I am monitoring the protocol status using the HAL_FDCAN_GetProtocolStatus function from the HAL library, but the error counter doesn't decrement, and the flags aren't resetting as they should.
Below is my CAN bus initialization and configuration routine:
void MX_FDCAN1_Init(void)
{
/* FDCAN1 parameter configuration */
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = ENABLE;
hfdcan1.Init.NominalPrescaler = 12;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 13;
hfdcan1.Init.NominalTimeSeg2 = 2;
hfdcan1.Init.DataPrescaler = 12;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 13;
hfdcan1.Init.DataTimeSeg2 = 2;
hfdcan1.Init.StdFiltersNbr = 0;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
}
/* CAN filter configuration */
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x0000;
sFilterConfig.FilterID2 = 0x0000;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
{
DebugPrint("Failed to config filter.");
}
/* Configure global filter to accept all frames */
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
DebugPrint("Failed to config global filter.");
}
/* Clearing Error Flags */
__HAL_FDCAN_CLEAR_FLAG(&hfdcan1, FDCAN_FLAG_ERROR_PASSIVE | FDCAN_FLAG_BUS_OFF);
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
DebugPrint("Failed to start FDCAN.");
}
/* Activate notifications */
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE | FDCAN_IT_ERROR_PASSIVE | FDCAN_IT_BUS_OFF, 0) != HAL_OK)
{
DebugPrint("Failed to activate notifications.");
}
I'm not sure if I'm missing a step or misconfiguring something. If anyone has suggestions or possible solutions for why the Bus-Off state isn't recovering, I'd greatly appreciate the help.
“Even the best fall down sometimes,” but I'd love to get this one sorted out soon. Thank you in advance!