CAN communication (no data visible on CAN HIGH or CAN LOW side of transciver TJA1050)
Hi all
I am trying to run CAN communication (normal mode ) from my discovery board (STM32F407) to USB CAN analyzer via (TJA1050).
I am able to see data on TJA1050 (CAN TX and RX side ) but no data is reflecting on CAN high and CAN low side, so because of no data is showing on CANH and CANL ,no data is reflecting on USB display (note: only rev led is blinking on USB CANAlyzer)
what can be issue ?
B.R
Ashish
PFA attached
CAN