Can COMP7\ETR1 reset TIM20 on only one edge instead of both?
I have TIM20 configured in reset mode and I want the output of COMP7 to reset it. I have TIM20 configured with ETR routed to COMP7 and I can see the timer being reset on both of the edges of the COMP7 signal. I only want TIM20 reset on one edge.
I'm using CubeIDE and I see options for choosing rising\falling\both for input capture, but no way to do it when routing from the internal comparators. Is this possible?