Question
Can I implement a nanosecond delayed signal output with the stm32H723 chip
- December 16, 2025
- 8 replies
- 141 views
I would like to implement delay signal output with STM32 MCU.
So I use the original signal input for EXT interrupt.
EXT interrupt's callback activates the timer
If a timer callback is called after a time delay of the desired value, it is implemented by setting the GPIO pin to HIGH.
However, it can be confirmed that the desired amount of delay is achieved, but the timing of the pin becoming HIGH varies each time, and it takes about 1.5 to 1.8us between EXT and TIMER.
I would like to know if the idea can be implemented as STM32 MCU series.
also posting my Clock Configuration pic