Can I use the STM32L433RCT6P without the external SMPS ?
I have designed a PCB that uses the STM32L433RCT6P which is the same processor used on the NUCLEO-L433RC-P board.
However, I am not using the external SMPS on the PCB I have designed.
I put up a post asking what I should do with the VDD12 pins if I dont use the external SMPS and was told to leave them floating (see https://community.st.com/t5/stm32-mcus-products/stm32l433rct-vdd12-pins-what-should-i-do-with-them/td-p/817459) so assumed I could use this MCU without the external SMPS.
My PCB is about to start production and now I am very concerned that the STM32L433RCT6P will not work without the external SMPS, is this true ?
If so I need to cancel production asap so a quick answer would be greatly appreciated.
My schematic is below for reference...

If the STM32L433RCT6P can be used without the external SMPS, is there a setting somewhere to tell it to use the internal LDO ?
During the design I did change to the non-P version (STM32L433RCT6) but I wanted to continue developing softwarea on the NUCLEO-L433RC-P board until my custom PCB arrived, so I reverted back to the STM32L433RCT6P