Can STM32 DMA chaining be used so that the end of a DMA transfer starts another on a different channel?
I think from what I've read this should be possible, but before diving into the details and trying to make it work I'm hoping someone can just give me a yes/no answer for this question. Basically, what I'm trying to do is use DMA to send a block of SPI data and when that block is done start another DMA transfer on another channel sending a very short block of data to a GPIO port BSRR register to toggle some I/O pins and when that block is done restart the first DMA transfer of SPI data. The idea is that the SPI data followed by the toggling of a few I/O pins (all on the same GPIO port, through a sequence) in an infinite high speed loop. Can MDMA be used to make this happen on an STM32 micro?
Thanks.