can't connect to hoverboard stm32f103rct6
Hi! I want to connect to old hoverboard but I can't make connection to mcu. I don't have idea why. I try a lot things but nothing worked. The chip is stm32f103rct6.
10:20:01 : UR connection mode is defined with the HWrst reset mode
10:20:01 : ST-LINK SN : B55B5A1A000000009532F001
10:20:01 : ST-LINK FW : V2J43S7
10:20:01 : Board : --
10:20:01 : Voltage : 3.25V
10:20:01 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication