Can't enable and disable writing in MT25QL512 external flash memory
Hello, everyone. I am developing a prototype using a STM32L475 and the NOR flash memory MT25QL512ABB. I am using the QuadSPI peripheral for the communication with these parameters:

I used the QSPI_ReadWrite_IT example as a reference to fill these parameters. When I try to send the commanda to enable or disable memory writing commands, the DQ1 pin stays in high state. Every time I try to send write enable (0x06) or write disable (0x04), the command turns into 0x26 due to DQ1 high as shown below:

I used a debugger and saw that the QuadSPI CCR register right before the command is sent has the right value. I also accessed the memory registers in quad mode to see their content:
Registers data:
STATUS REGISTER (0x05): 0x00
Status register write enable/disable: 0
Write enable latch: 0
Write in progress: 0
FLAG STATUS REGISTER (0x70): 0x80
Program or erase controller: 1
Erase suspend: 0
Erase: 0
Program: 0
Program suspend: 0
Protection: 0
Addressing (3 or 4 bytes): 0
NONVOLATILE CONFIGURATION REGISTER (0xB5): 0xFF 0xFF
Double transfer rate protocol (E/D): 1
Reset/hold (E/D): 1
Quad I/O protocol (E/D): 1
Dual I/O protocol (E/D): 1
Number of address bytes during command entry (4 or 3 bytes): 1
VOLATILE CONFIGURATION REGISTER (0x85): 0xFB
ENHANCED VOLATILE CONFIGURATION REGISTER (0x65): 0x7F
Quad I/0 protocol (E/D): 0
Dual I/O protocol (E/D): 1
Double transfer rate protocol (E/D): 1
Reset/hold (E/D): 1
EXTENDED ADDRESS REGISTER (0xC8): 0x00
I also noticed that the DQ1 is not following the same behavior comparing with the other pins. I included the Write enable command after reading each register and right before the read command, DQ1 goes low (and change its state to send the right read register command) and after trying to send the write enable command, DQ1 stays in High state. Doing this, I can't read the registers data properly as well.

I tried sending these writing enable and disable commands in all modes, but I wasn't able to change the write enable latch in the status register. Another huge problem is that I can run the same code within the STM32G474VET and the same memory type and it runs perfectly as shown below: