Can the array DAC DMA for signals be controlled?
I generated a sinusoidal signal through the DAC using DMA. I understand that DMA performs looping since I use circular mode. In short, I want to control the numbers generated by the DMA. So, when the signal changes to DC (the array contains only 2048 or hold_samples and hold_samples2), it will immediately be detected by my program using the function:
deteksisinyal(void)
However, I have NOT yet figured out how to control the numbers/results/shape of the generated signal in terms of code. I want to control the signal changes, namely from peak - flat - valley - flat. I will use the flat part for another function, specifically to detect changes in a device. Please, I need help from experts with examples or guidance on what I should do. I will include my code below. Please provide feedback or ask questions about my code.
// DAC SIGNAL GENERATOR
#define VALUE_SIZE 557
uint16_t value[VALUE_SIZE] = {};
uint16_t hold_samples = 30;
uint16_t hold_samples2 = 400;
uint16_t firstHalf[] = {
2100, 2249, 2450, 2646, 2834, 3018, 3188, 3351, 3503, 3636, 3755, 3860, 3944, 4012, 4095,
4058, 4012, 3944, 3860, 3755, 3636, 3503, 3351, 3188, 3018, 2834, 2646, 2450, 2249, 2100
};
uint16_t secondHalf[] = {
1997, 1847, 1702, 1562, 1427, 1297, 1172, 1052, 900, 722, 622, 527, 437, 352, 272, 197, 100,
0, 100, 197, 272, 352, 437, 527, 622, 722, 900, 1052, 1172, 1297, 1427, 1562, 1700, 1850, 2000
};
// ADC SIGNAL GENERATOR
uint16_t totalSize;
uint16_t sum_signal = 0;
uint16_t filtered_input; //ngantuk bgt ya lord
void generate_signal() {
uint16_t index = 0;
for (uint16_t i = 0; i < sizeof(firstHalf) / sizeof(firstHalf[0]); i++) {
value[index++] = firstHalf[i];
}
for (uint16_t i = 0; i < hold_samples; i++) {
value[index++] = 2048;
}
for (uint16_t i = 0; i < sizeof(secondHalf) / sizeof(secondHalf[0]); i++) {
value[index++] = secondHalf[i];
}
for (uint16_t i = 0; i < hold_samples2; i++) {
value[index++] = 2048;
}
totalSize = (sizeof(firstHalf) / sizeof(firstHalf[0])) + hold_samples + (sizeof(secondHalf) / sizeof(secondHalf[0]))+ hold_samples2;
HAL_DAC_Start_DMA(&hdac, DAC_CHANNEL_1, (uint32_t*)value, totalSize, DAC_ALIGN_12B_R);
}
uint32_t cnt=0;
uint16_t input_start = 0;
uint32_t input_end = 4095;
uint16_t output_start = 25;
uint16_t output_end = 3900;
uint16_t newArray = 2048;
uint16_t input;
uint16_t hasil;
uint16_t i;
uint16_t y;
uint16_t x;
uint16_t newArray;
void signal_function(){
input = adc_buffer[1];
cnt++;
if (cnt > 15)
{
filtered_input = sum_signal / 15;
sum_signal=0;
cnt=0;
hasil = output_start + ((output_end - output_start) * (filtered_input - input_start)) / (input_end - input_start);
__HAL_TIM_SET_AUTORELOAD(&htim4, hasil);
__HAL_TIM_SET_COMPARE(&htim4, TIM_CHANNEL_1, hasil);
y = hasil;
x = input;
}
else
sum_signal += input;
}
void deteksisinyal(void){
//how to detect the DC signallllll
}
and the shape of the signal is as follows:
and the shape of the signal is as follows:
Is it possible? I need your help.