Can USB CDC_Receive_FS Callback be called more than once
Hello,
I've enabled a USB virtual com port on an STM32F373 successfully. The CDC_Receive_FS function in usbd_cdc_if.c gets called when data is received. I never expect to never receive a 'packet' greater than 64 bytes and have created my USB buffer[64] variable accordingly.
My questions is can I ever expect CDC_Receive_FS to be called more than once in some cases, even if the sender is always transmitting a 'packet' less than 64 bytes? I know my UART RX callback sometimes gets called more than once, with the 'packet' split into 2 callbacks. Will CDC_Receive_FS act the same way or can I rest assured *Len will always equal the exact number of bytes transmitted by the sender in 1 'packet'?
I currently consider anything sent between 'idle' times of 1 byte or more to be a 'packet'.
Thank you