Can USB CDC receive more than 256 bytes of data from the host?
Hi everyone.
I'm trying to send more than 256 bytes of data from the host to the STM32 using USB CDC VCP, and I don't know why VCP won't accept more than 64 bytes of data. My project is already halfway done. If I switch to the USB bulk method, do I have to replace the USB CDC library and rewrite all the code from scratch? And do I have to create my own library to replace USB CDC?
I'm using an STM32F407VET6.
I appreciate all your answers.
Thank you:).