Question
Can VDDA VREF+ and VssA connect to VSS(ground)?
I am using STM32H735,TFBGA-100 controller with 550MHz.I don't need ADC and DAC functions.
1.Shall i connect VDDA,VREF+ and VssA to ground(Vss)? if yes, what is the recommended(through any resistor or shorted)way to connect to Vss?
2.If i did as above, what are consequences?
3.Does it effect RESET function of controller?