Canbus callback not working on stm32f429
Hi amazing community.
I am working with stm32f429 and cube ide.
This is my configuration for the project


/**
* @brief CAN1 Initialization Function
* None
* @retval None
*/
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 18;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = ENABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = ENABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
/* USER CODE END CAN1_Init 2 */
}

With the configuration above i am not able to enter inside the following callback funxtion sending messages wit canbus
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
CAN_RxHeaderTypeDef header;
uint8_t data[8];
uint32_t cmd_id;
if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &header, data) == HAL_OK)
{
if ((can_dev.rx_queue_in+1)%CAN_RX_QUEUE != can_dev.rx_queue_out && header.IDE == CAN_ID_EXT)
{
// filtro messaggi destinati al nodo
cmd_id = header.ExtId;
if (cmd_id == can_dev.cfg_id || (can_dev.base != 0 &&
(
cmd_id == can_dev.base + can_dev.rec_offset*MSG_CFG_STATUS ||
cmd_id == can_dev.base + can_dev.rec_offset*MSG_OUT_ENABLE ||
cmd_id == can_dev.base + can_dev.rec_offset*MSG_INP_ENABLE ||
cmd_id == can_dev.base + can_dev.rec_offset*MSG_HW_VER ||
cmd_id == can_dev.base + can_dev.rec_offset*MSG_FW_VER ||
cmd_id == can_dev.base + can_dev.rec_offset*MSG_OUT_FREE
))) {
can_dev.rx++;
memcpy(&can_dev.rx_msg_queue[can_dev.rx_queue_in].header, &header, sizeof(CAN_RxHeaderTypeDef));
memcpy(can_dev.rx_msg_queue[can_dev.rx_queue_in].data, data, sizeof(data));
can_dev.rx_queue_in = (can_dev.rx_queue_in + 1) % CAN_RX_QUEUE;
}
}
can_dev.error_glb = 0;
can_dev.tot_rx++;
}
}
Can you please tell me if you see mistakes in the configuration or something else ?
Thanks a lot