Cannot enter DFU mode on STM32F446ZET6
Hi everyone,
I’m working with a custom made STM32F446ZET6 board that otherwise functions perfectly (all peripherals, flash programming, etc. work fine). The only thing that doesn’t is the ROM bootloader. I can’t get USB DFU or UART boot to respond no matter what I do.
What I’ve verified
-
BOOT0 = 1 (3.3 V) at reset
-
NRST pulled high, no reset loops
-
VDDUSB = 3.3 V, decoupled with 100 nF
-
HSE = Abracon ABLS-8 MHz-12 pF, started with 18 pF load caps and lowered to 10 pF as I saw in a post here this might be the cause
-
PA9 connected directly to VBUS (5 V)
-
PA11/PA12 wired to USB-FS D−/D+ (verified routing and continuity)
-
Board runs normal firmware from Flash with no issues
What I’ve tried
-
BOOT0=1, reset → USB never enumerates
-
Tried UART boot (PA10 RX, PA9 TX, 115200 8E1) → no ACK, completely silent.
-
Verified with ST-Link under reset:
-
RDP = 0xAA (no protection)
-
MEMRMP = 0x0, VTOR = 0x0 → seems like it’s still mapping main Flash, not System Memory.
-
-
Jumped to 0x1FFF0000 manually via GDB/OpenOCD:
-
Program counter at 0x1FFF503C, D+ line goes high, so bootloader code definitely runs.
-
But USB still doesn’t enumerate.
-
Observations
-
D+ rises high after the jump (so FS pull-up activates), but host never recognizes the device.
-
Everything else on the board, including USB device mode under firmware (Marlin/ Klipper) works fine.
Questions
-
What could cause the internal System Memory bootloader not to fully start USB DFU or UART?
-
Is there any condition (clock, pin, option byte, etc.) that can block the ROM bootloader on F4 from initializing peripherals?
-
Has anyone seen a case where the bootloader starts (D+ goes high) but host never enumerates?
-
Any other hardware requirement besides VBUS > 4 V on PA9 and VDDUSB = 3.3 V that could prevent enumeration?
Any insights would be appreciated. I can share schematics or test logs if needed.
Thanks,